Keysight 89600 VSA .NET API
ElementSpacingInVerticalDirection Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : ElementSpacingInVerticalDirection Property


Glossary Item Box

Gets or sets the distance between the adjacent elements within the same antenna panel in the vertical direction.

Syntax

Visual Basic (Declaration) 
Public Property ElementSpacingInVerticalDirection As Double
C# 
public double ElementSpacingInVerticalDirection {get; set;}
C++/CLI 
public:
property double ElementSpacingInVerticalDirection {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also