Keysight 89600 VSA .NET API
PanelSpacingInHorizontalDirection Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : PanelSpacingInHorizontalDirection Property


Glossary Item Box

Gets or sets the distance between the adjacent panels in the horizontal direction.

Syntax

Visual Basic (Declaration) 
Public Property PanelSpacingInHorizontalDirection As Double
C# 
public double PanelSpacingInHorizontalDirection {get; set;}
C++/CLI 
public:
property double PanelSpacingInHorizontalDirection {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also