Keysight 89600 VSA .NET API
RectangularAntennaPanelArray Constructor
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > RectangularAntennaPanelArray Class : RectangularAntennaPanelArray Constructor


Glossary Item Box

Overload List

OverloadDescription
RectangularAntennaPanelArray Constructor()Initializes a new instance of the RectangularAntennaPanelArray class with default settings.  
RectangularAntennaPanelArray Constructor(Double,ElementSpacingUnit,Int32,Int32,Int32,Double,Double,Int32,Int32,Double,Double)Initializes a new instance of the RectangularAntennaPanelArray class with the specified settings.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also