| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsGridEnabled As Boolean | |
| C# | |
|---|---|
public abstract bool IsGridEnabled {get; set;} | |
The default value depends on the index of this resource grid in the ResourceGridCollection. The default value is true if the index is 1. Otherwise, it is false. Index 0 represents Mu0:15kHz. Index 1 represents Mu1:30kHz. Index 2 represents Mu2:60kHz. Index 3 represents Mu3:120kHz. Index 4 represents Mu4:240kHz. If a resource grid is invalid, it is disabled.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)