| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property HalfFrameIndex As Integer | |
| C# | |
|---|---|
public virtual int HalfFrameIndex {get; set;} | |
The value can be 0 or 1. when it is 0, SSB block starts from the first half frame boundary, and if it is 1, the SSB block starts from the second half frame boundary.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00