Keysight 89600 VSA .NET API
SSBlock Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SSBlock Class

Glossary Item Box

The following tables list the members exposed by SSBlock.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActiveIndexesGets or sets the indexes (zero-based) on which the SS/PBCH physical channels are reserved.  —
Public PropertyAutoDetectActiveBlocksOnGets or sets a value indicating whether to auto detect which SS/PBCH blocks are active.  —
Public PropertyAutoDetectPowerThresholdGets or sets the power threshold (in dB, relative to maximum SS/PBCH block power) to use to decide if an SS/PBCH block is active.  —
Public PropertyHalfFrameIndexGets or sets the value indicating the half frame index the SSB block starts with when the SSB block period is not 5 milliseconds.  26.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsSSBlockEnabledGets or sets a value indicating whether this resource allocation is currently applied to the ComponentCarrier .  —
Public PropertyLmaxGets or sets the maximum number of possible SS/PBCH blocks in a transmission opportunity.  —
Public PropertyNumerologyGets or sets a value indicating the numerology for this resource allocation.  —
Public PropertyPbchGets a reference to the PBCH physical channel settings.  —
Public PropertyPeriodicityGets or sets a value indicating the SS/PBCH resource allocation periodicity.  —
Public PropertyPssGets a reference to the PSS physical channel settings.  —
Public PropertyRBNumberGets a value indicating the number of RB available in this resource allocation.  —
Public PropertyRBOffsetGets or sets a value indicating the RB Offset for this resource allocation.  —
Public PropertySssGets a reference to the SSS physical channel settings.  —
Public PropertySubcarrierOffsetGets or sets the subcarrier offset of the SS/PBCH block relative to the RBOffset.  —
Public PropertySubcarrierSpacingCommonGets or sets the subcarrier spacing used for the SubcarrierOffset when ssb numerology is 120kHz or 240kHz.  24.20
Public PropertySymbolStartForMu1Gets or sets the symbol start equation used when the numerology is 30 kHz (µ = 1)  —
Public PropertyVersionGets or sets the specification interpretation to use for SS/PBCH.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also