Keysight 89600 VSA .NET API
CoresetId Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SearchSpace Class : CoresetId Property


Glossary Item Box

Gets or sets coreset id to be analyzed.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CoresetId As Integer
C# 
public virtual int CoresetId {get; set;}
C++/CLI 
public:
virtual property int CoresetId {
   int get();
   void set (    int value);
}

Remarks

Default value is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also