Keysight 89600 VSA .NET API
SearchSpace Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SearchSpace Class

Glossary Item Box

The following tables list the members exposed by SearchSpace.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyCandidateNumber1Gets or sets the number of candidates for aggregation level 1.  —
Public PropertyCandidateNumber16Gets or sets the number of candidates for aggregation level 16.  —
Public PropertyCandidateNumber2Gets or sets the number of candidates for aggregation level 2.  —
Public PropertyCandidateNumber4Gets or sets the number of candidates for aggregation level 4.  —
Public PropertyCandidateNumber8Gets or sets the number of candidates for aggregation level 8.  —
Public PropertyCoresetIdGets or sets coreset id to be analyzed.  —
Public PropertyFlexibleSymbolsGets or sets the flexible symbols to be used in the slot format.  24.20
Public PropertyFramePeriodGets or sets a value indicating the period (in number of frames) when the slot allocation repeats.  26.20
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertySearchSpaceTypeGets or sets search space type.  —
Public PropertySfiGets or sets the slot format indicator used for this search space.  24.20
Public PropertySymbolStartGets or sets monitor symbol starting index  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetAllocatedSlotIndexesGets the set of slot indexes allocated for this physical channel.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetSfiDescriptionGets the slot format indicator detailed description indicating the symbol directions.  24.20
Public MethodGetSfiSymbolDirectionsGets the slot format indicator symbol directions.  24.20
Public MethodGetValidSfiValuesGet the valid slot format indicator values.  24.20
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetAllocatedSlotIndexesOverloaded. Sets a single contiguous set of slots to be allocated for this physical channel.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also