| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property FlexibleSymbols As Integer | |
| C# | |
|---|---|
public virtual int FlexibleSymbols {get; set;} | |
Property Value
The default is 0, indicating no "Flexible" symbols should be allocated to this physical channel.This property helps define the set of symbols reserved for this search space. This value represents a bitmap to indicate which "Flexible" symbols from the Sfi should be available to this search space (in every slot). This is applied in coordination with Sfi.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20