Keysight 89600 VSA .NET API
FramePeriod Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SearchSpace Class : FramePeriod Property


Glossary Item Box

Gets or sets a value indicating the period (in number of frames) when the slot allocation repeats.

Syntax

Visual Basic (Declaration) 
Public Overridable Property FramePeriod As Integer
C# 
public virtual int FramePeriod {get; set;}
C++/CLI 
public:
virtual property int FramePeriod {
   int get();
   void set (    int value);
}

Property Value

Default value is 1 frame. Range is from 1 to 16 frames.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also