Keysight 89600 VSA .NET API
SymbolStart Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > SearchSpace Class : SymbolStart Property


Glossary Item Box

Gets or sets monitor symbol starting index

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SymbolStart As Integer
C# 
public abstract int SymbolStart {get; set;}
C++/CLI 
public:
abstract property int SymbolStart {
   int get();
   void set (    int value);
}

Property Value

Default value is 0. Range of value is 0 through 13.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also