Keysight 89600 VSA .NET API
SfiSymbolDirection Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SfiSymbolDirection Enumeration


Glossary Item Box

Enum values indicating the symbol direction in the slot format.

Syntax

Visual Basic (Declaration) 
Public Enum SfiSymbolDirection 
   Inherits System.Enum
C# 
public enum SfiSymbolDirection : System.Enum 
C++/CLI 
public enum class SfiSymbolDirection : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DownlinkSymbol in slot format is downlink.—
FlexibleSymbol in slot format is flexible.—
UplinkSymbol in slot format is uplink.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also