Keysight 89600 VSA .NET API
AntennaPort Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : AntennaPort Property


Glossary Item Box

Gets or sets a value indicating the antenna port of this physical channel to be analyzed.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AntennaPort As SrsAntennaPort
C# 
public abstract SrsAntennaPort AntennaPort {get; set;}
C++/CLI 
public:
abstract property SrsAntennaPort AntennaPort {
   SrsAntennaPort get();
   void set (    SrsAntennaPort value);
}

Property Value

If equals to , valid SRS antenna port is ; If equals to , valid SRS antenna port is and ; If equals to , valid SRS antenna port is , , and ; The default value is .

Remarks

Currently SRS antenna port auto detection is not supported yet, this parameter tells VSA which antenna port is to be analyzed. .

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also