Keysight 89600 VSA .NET API
NumberOfSymbols Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : NumberOfSymbols Property


Glossary Item Box

Gets or sets a value indicating the number of SRS symbols in the slot.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NumberOfSymbols As NumberOfSrsSymbols
C# 
public abstract NumberOfSrsSymbols NumberOfSymbols {get; set;}
C++/CLI 
public:
abstract property NumberOfSrsSymbols NumberOfSymbols {
   NumberOfSrsSymbols get();
   void set (    NumberOfSrsSymbols value);
}

Property Value

The SRS symbol number can 1 or 2 or 4. The default value is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also