Keysight 89600 VSA .NET API
SlotPeriod Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Srs Class : SlotPeriod Property


Glossary Item Box

Gets or sets the SRS Slot period

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SlotPeriod As Integer
C# 
public abstract int SlotPeriod {get; set;}
C++/CLI 
public:
abstract property int SlotPeriod {
   int get();
   void set (    int value);
}

Remarks

When is or , this value decides the slot period on which this SRS is transmitted.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also