| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property ResourceType As SrsResourceType | |
| C# | |
|---|---|
public abstract SrsResourceType ResourceType {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property SrsResourceType ResourceType { SrsResourceType get(); void set ( SrsResourceType value); } | |
Property Value
The default value is SrsResourceType.CustomDefinedThis value decides how this SRS resource is allocated on the specified slots, . When it is , this SRS is transmitted on the slots , and it is only transmitted once. When it is , this SRS is transmitted on slot every slots. When it is , this SRS is transmitted on slot every slots as long as this SRS resource is activated. When it is , this SRS is transmitted on the slots , and it is transmitted in every frame.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00