Keysight 89600 VSA .NET API
SynchronizationTechnique Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SynchronizationTechnique Enumeration


Glossary Item Box

Enum values indicating the synchronization technique applied during analysis.

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationTechnique 
   Inherits System.Enum
C# 
public enum SynchronizationTechnique : System.Enum 
C++/CLI 
public enum class SynchronizationTechnique : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CPAutocorrelationFrequency domain synchronization strategy using cyclic-prefix correlation.—
TimeCrossCorrelationTime domain cross correlation synchronization strategy.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The analyzer attempts to align the measured signal with the location specified by MeasurementExtension.AnalysisStartBoundary. This setting modifies the search algorithm used by the analyzer. If CPAutocorrelation is selected, a frequency domain synchronization strategy using cyclic-prefix correlation is used. This approach typically results in a faster measurement. If TimeCrossCorrelation is selected, a time domain cross correlation synchronization strategy is used. This approach typically results in higher probability of synchronization for noisy signal conditions.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also