Keysight 89600 VSA .NET API
BaseStationCategory Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : BaseStationCategory Enumeration


Glossary Item Box

Enum values indicating the base station category.

Syntax

Visual Basic (Declaration) 
Public Enum BaseStationCategory 
   Inherits System.Enum
C# 
public enum BaseStationCategory : System.Enum 
C++/CLI 
public enum class BaseStationCategory : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ALocalAreaBase station category A with local area—
AMediumRangeBase station category A with medium range—
AMediumRangeLowPowerRatedBase station category A with medium range (low power rated)—
AWideAreaBase station category A with wide area—
BLocalAreaBase station category B with local area—
BMediumRangeBase station category B with medium range—
BMediumRangeLowPowerRatedBase station category B with medium range (low power rated)—
BWideAreaBase station category B with wide area—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also