Keysight 89600 VSA .NET API
Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace
See Also  Inheritance Hierarchy
Agilent.SA.Vsa.NewRadio.Interfaces Assembly : Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace

Glossary Item Box

Classes

 ClassDescription
ClassCalculationControl The CalculationControl represents the measurement control for the DirectCalculation.
ClassCalculationResult The CalculationResult contains all the possible results provided by the DirectCalculation.
ClassCarrierConfiguration Defines a component carrier configuration.
ClassCarrierConfigurationCollection This class represents a collection of carrier configuration instances
ClassConfigurationResult The ConfigurationResult represents the results of the configure operation of the DirectCalculation.
ClassNewRadioContextExtension A Keysight.SA.Vsa.ContextExtension for configuring a 5G New Radio signal.
ClassNewRadioDirectCalculation This class provides the members required to configure and control a DirectCalculation.
ClassRequirementsForOfdmDomainInputData The RequirementsForOfdmDomainInputData represents the requirements for the ofdm domain input data.
ClassStandardSpecificConfiguration The standard specific configuration represents the setup configuration used in determining the proper new radio configuration to apply.

Enumerations

 EnumerationDescription
EnumerationAllocationMode Enum values indicating how carriers are allocated.
EnumerationAssumedAdjacentChannel Enum values indicating the assumed adjacent channel
EnumerationBaseStationCategory Enum values indicating the base station category.
EnumerationBaseStationType Enum values indicating the test setup of the base station.
EnumerationChannelRaster Enum values indicated the channel raster.
EnumerationChannelSpacing Enum values indicated the channel spacing.
EnumerationFrequencyRangeLimitMask Enum values indicating the frequency range to use for the limit mask.
EnumerationInputDataDomain Enum values indicating the input data domain for DirectCalculation.
EnumerationSignalAcquisitionMode Enum values indicating how the signal acquisition is handled based on the frequency regions defined and the hardware's maximum IF bandwidth.
EnumerationUEPowerClass Enum values indicating the user-equipment power class
EnumerationUplinkChannelType Enum values indicating the uplink channel type

See Also