Keysight 89600 VSA .NET API
BaseStationType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : BaseStationType Enumeration


Glossary Item Box

Enum values indicating the test setup of the base station.

Syntax

Visual Basic (Declaration) 
Public Enum BaseStationType 
   Inherits System.Enum
C# 
public enum BaseStationType : System.Enum 
C++/CLI 
public enum class BaseStationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FR1ConductedBase station has a FR1 conducted setup—
FR1OtaBase station has a FR1 OTA setup—
FR2OtaBase station has a FR2 OTA setup—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also