Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace > CarrierConfigurationCollection Class : Remove Method


item
CarrierConfiguration to remove from the collection

Glossary Item Box

Removes the indicated CarrierConfiguration from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As CarrierConfiguration _
) As Boolean
C# 
public abstract bool Remove( 
   CarrierConfiguration item
)
C++/CLI 
public:
abstract bool Remove( 
   CarrierConfiguration^ item
) 

Parameters

item
CarrierConfiguration to remove from the collection

Return Value

True, if the CarrierConfiguration was removed from the collection. False otherwise.

Remarks

The maximum number of CarrierConfiguration items is 16, the minimum is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also