| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function RemoveAt( _ ByVal index As Integer _ ) As Boolean | |
Parameters
- index
- Zero-based index of user to remove from the collection
Return Value
True, if the CarrierConfiguration was removed from the collection. False otherwise.The maximum number of CarrierConfiguration items is 16, the minimum is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)