Keysight 89600 VSA .NET API
ChannelRaster Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : ChannelRaster Enumeration


Glossary Item Box

Enum values indicated the channel raster.

Syntax

Visual Basic (Declaration) 
Public Enum ChannelRaster 
   Inherits System.Enum
C# 
public enum ChannelRaster : System.Enum 
C++/CLI 
public enum class ChannelRaster : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FifteenKilohertzChannel raster is 15kHz—
NoneNo channel raster is used.—
OneHundredKilohertzChannel raster is 100kHz—
SixtyKilohertzChannel raster is 60kHz—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also