Keysight 89600 VSA .NET API
ConfigurationResult Class Members
See Also  Properties 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : ConfigurationResult Class

Glossary Item Box

The following tables list the members exposed by ConfigurationResult.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorConfigurationResult ConstructorInitializes a new instance of the ConfigurationResult class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDemodResultLengthInSubframeGets the demodulation result length in subframes.  —
Public PropertyRequiredDelayPointsGets the number of input data pre-settling (delay) samples incurred during the configured measurement.  —
Public PropertyRequiredInputDataDomainGets the required input data domain.  —
Public PropertyRequiredInputDataPointsGets the total number of input data samples the user must supply in order to satisfy the configured measurement.  —
Public PropertyRequiredSampleRateForTimeDomainInputGets the required sample rate for time domain input data with unit of Hz.  —
Public PropertyRequiredSettlePointsGets the sum total of input data settling samples the user must supply in order to satisfy the configured measurement.  —
Public PropertyRequiredSignalFormatGets the required signal format.  —
Public PropertyRequirementsForOfdmDomainInputDataGets a reference to the requirements for the ofdm domain input data.  —
Public PropertyStatusGets the overall status after the configuration.  —
Public PropertyStatusMessagesGets the collection of all the status messages after the configuration.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also