| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function ConfigureWithVsaSetupFile( _ ByVal fileName As String, _ ByVal calculationControl As CalculationControl _ ) As ConfigurationResult | |
| C# | |
|---|---|
public abstract ConfigurationResult ConfigureWithVsaSetupFile( string fileName, CalculationControl calculationControl ) | |
| C++/CLI | |
|---|---|
public: abstract ConfigurationResult^ ConfigureWithVsaSetupFile( String^ fileName, CalculationControl^ calculationControl ) | |
Parameters
- fileName
- The VSA setx file name with full path
- calculationControl
- The control for this calculation
Return Value
ConfigurationResult is returned which includes the overall status, all the status messages, the signal format, and all the requirements for the input data.When the measurement extension defined in the setx file is not NewRadio, Keysight.SA.Vsa.OverallStatus.Error will be returned in ConfigurationResult.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)