Keysight 89600 VSA .NET API
RequirementsForOfdmDomainInputData Class Members
See Also  Properties 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : RequirementsForOfdmDomainInputData Class

Glossary Item Box

The following tables list the members exposed by RequirementsForOfdmDomainInputData.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorRequirementsForOfdmDomainInputData ConstructorInitializes a new instance of the RequirementsForOfdmDomainInputData class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyFirstSubcarrierIndexGets the required first subcarrier index.  —
Public PropertyFirstSymbolIndexGets the required first symbol index.  —
Public PropertyNumberOfSubcarriersGets the required number of subcarriers.  —
Public PropertyNumberOfSymbolsGets the required number of symbols.  —
Public PropertySubcarrierSpacingGets the required subcarrier spacing.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also