Keysight 89600 VSA .NET API
SignalAcquisitionMode Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : SignalAcquisitionMode Enumeration


Glossary Item Box

Enum values indicating how the signal acquisition is handled based on the frequency regions defined and the hardware's maximum IF bandwidth.

Syntax

Visual Basic (Declaration) 
Public Enum SignalAcquisitionMode 
   Inherits System.Enum
C# 
public enum SignalAcquisitionMode : System.Enum 
C++/CLI 
public enum class SignalAcquisitionMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutoAutomatically handles acquisition behavior.—
MultibandSequentialAcquisitionLeverages sequential acquisitions to create a spectrum per frequency region.—
SingleAcquisitionUses a single acquisition to capture frequency regions, and restricts regions that exceed beyond the max bandwidth of the hardware by disabling the region.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also