Keysight 89600 VSA .NET API
UEPowerClass Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Keysight.SA.Vsa.ContextExtensions.NewRadio Namespace : UEPowerClass Enumeration


Glossary Item Box

Enum values indicating the user-equipment power class

Syntax

Visual Basic (Declaration) 
Public Enum UEPowerClass 
   Inherits System.Enum
C# 
public enum UEPowerClass : System.Enum 
C++/CLI 
public enum class UEPowerClass : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FourUE power is class 4.—
OneUE power is class 1.—
ThreeUE power is class 3.—
TwoUE power is class 2.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also