Keysight 89600 VSA .NET API
DeinterleaveEmitterSelections Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : DeinterleaveEmitterSelections Enumeration


Glossary Item Box

Specifies which emitters deinterleaving is enabled on.

Syntax

Visual Basic (Declaration) 
Public Enum DeinterleaveEmitterSelections 
   Inherits System.Enum
C# 
public enum DeinterleaveEmitterSelections : System.Enum 
C++/CLI 
public enum class DeinterleaveEmitterSelections : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Emitter1Deinterleaving is enabled on emitter1—
Emitter10Deinterleaving is enabled on emitter1024.20
Emitter11Deinterleaving is enabled on emitter1124.20
Emitter12Deinterleaving is enabled on emitter1224.20
Emitter13Deinterleaving is enabled on emitter1324.20
Emitter14Deinterleaving is enabled on emitter1424.20
Emitter15Deinterleaving is enabled on emitter1524.20
Emitter16Deinterleaving is enabled on emitter1624.20
Emitter17Deinterleaving is enabled on emitter1724.20
Emitter18Deinterleaving is enabled on emitter1824.20
Emitter19Deinterleaving is enabled on emitter1924.20
Emitter2Deinterleaving is enabled on emitter2—
Emitter20Deinterleaving is enabled on emitter2024.20
Emitter21Deinterleaving is enabled on emitter2124.20
Emitter22Deinterleaving is enabled on emitter2224.20
Emitter23Deinterleaving is enabled on emitter2324.20
Emitter24Deinterleaving is enabled on emitter2424.20
Emitter25Deinterleaving is enabled on emitter2524.20
Emitter26Deinterleaving is enabled on emitter2624.20
Emitter27Deinterleaving is enabled on emitter2724.20
Emitter28Deinterleaving is enabled on emitter2824.20
Emitter29Deinterleaving is enabled on emitter2924.20
Emitter3Deinterleaving is enabled on emitter3—
Emitter30Deinterleaving is enabled on emitter3024.20
Emitter4Deinterleaving is enabled on emitter4—
Emitter5Deinterleaving is enabled on emitter524.20
Emitter6Deinterleaving is enabled on emitter624.20
Emitter7Deinterleaving is enabled on emitter724.20
Emitter8Deinterleaving is enabled on emitter824.20
Emitter9Deinterleaving is enabled on emitter924.20
NoneDeinterleaving is disabled on all emitters.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also