| Class | Description | |
|---|---|---|
![]() | AngleOfArrival | Settings for angle of arrival analysis. |
![]() | AoaAntenna | Settings for positioning of the angle of arrival antenna. |
![]() | AoaAntennaCollection | This class represents a collection of AoaAntenna instances. |
![]() | HopAnalysis | Settings for frequency hopping analysis. |
![]() | HopAnalysisState | The HoppingAnalysisState represents a single state in a frequency hopping sequence. |
![]() | MeasurementExtension | The Pulse.MeasurementExtension object contains properties and members to control Pulse Analysis. |
![]() | NonlinearFM | Setting for Nonlinear FM modulation support. |
![]() | TrainBaseError | Gets the settings for a train's base error metrics. |
![]() | TrainReferencePulse | Settings for a train's reference pulse. |
![]() | TrainReferencePulseCollection | This class represents a collection of TrainReferencePulse instances. |
![]() | TrainScoring | Settings for individual train scoring. |
![]() | TrainScoringCollection | This class represents a collection of TrainScoring instances. |
![]() | TrainSearch | Settings for Pulse Train Search analysis. |
| Enumeration | Description | |
|---|---|---|
![]() | AmplitudeDomain | Domain for rise/fall/pulse width thresholds and used in percent droop, overshoot, and ripple calculations. |
![]() | AoaAnalysisMode | Specifies the analysis type for Angle Of Arrival (AOA). |
![]() | AoaAntennaOrientation | Specifies the antenna orientation for the angle of arrival measurement. |
![]() | AoaFrequencyMode | Specifies the reference frequency for Angle Of Arrival (AOA) Calculation. |
![]() | DeinterleaveEmitterSelections | Specifies which emitters deinterleaving is enabled on. |
![]() | DeinterleaveModulation | Specifies the modulation type to deinterleave with. |
![]() | DetectionThresholdReference | Specifies whether the pulse detection threshold value is relative or absolute. |
![]() | FrequencyReportMode | Specifies whether to show absolute or relative frequency values in result tables. |
![]() | HistogramRangeSelection | Specifies the mode for calculating the left and right x-axis limits of histograms. |
![]() | HopStateDetectionMode | Determines how frequency hop state detection occurs in the measurement. |
![]() | MeasurementPauseOperator | Measurement Pause operators for comparing the measured value to the user-specified threshold. |
![]() | NonlinearFMNormalization | Determines the region of the pulse to normalize. |
![]() | PulseExportMode | Determines whether to export the entire recording or just the current measurement results. |
![]() | PulseTimeStartReportMode | Specifies how time values are reported in traces and result tables. |
![]() | PulseToPulseAnalysisReference | Specifies the location of the pulse-to-pulse analysis time window. |
![]() | SelectedPulsesPart | Parts of the pulse to show and highlight. |
![]() | SidelobeKeepOutMode | Specify the sidelobe keep-out mode. |
![]() | TableMetric | Metrics which can appear in the Pulse Table. |
![]() | TdoaTimeReferenceMode | Specifies the reference timing for Time Difference Of Arrival (TDOA). |
![]() | TopBaseCalculationMethod | Methods for calculating the top and base levels of pulses. |
![]() | TrainSearchModulationType | Specifies the modulation type for train search scoring. |