Keysight 89600 VSA .NET API
DetectionThresholdReference Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : DetectionThresholdReference Enumeration


Glossary Item Box

Specifies whether the pulse detection threshold value is relative or absolute.

Syntax

Visual Basic (Declaration) 
Public Enum DetectionThresholdReference 
   Inherits System.Enum
C# 
public enum DetectionThresholdReference : System.Enum 
C++/CLI 
public enum class DetectionThresholdReference : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AbsoluteAllows user to specify desired Pulse Detection Threshold (dBm) level directly as an absolute Threshold (dBm) level.—
RelativeToBaseAllows user to specify desired Pulse Detection Threshold (dBm) level as a relative Threshold (dB) offset from measured acquisition Base Level (dBm) observed over entire Acquisition Length.—
RelativeToRangeAllows user to specify desired Pulse Detection Threshold (dBm) level as a relative Threshold (dB) offset from currently selected Input Range (dBm) level.—
RelativeToTopAllows user to specify desired Pulse Detection Threshold (dBm) level as a relative Threshold (dB) offset from measured acquisition Top Level (dBm) observed over the entire Acquisition Length.—
TriggerLevelAllows user to specify desired Pulse Detection Threshold (dBm) level as equal to the measurement's trigger level.20.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also