Keysight 89600 VSA .NET API
FrequencyReportMode Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : FrequencyReportMode Enumeration


Glossary Item Box

Specifies whether to show absolute or relative frequency values in result tables.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyReportMode 
   Inherits System.Enum
C# 
public enum FrequencyReportMode : System.Enum 
C++/CLI 
public enum class FrequencyReportMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AbsoluteFrequencies in result tables are absolute.—
RelativeToCenterFrequencies in result tables are relative to the measurement center frequency.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also