Keysight 89600 VSA .NET API
HopAnalysisState Class Members
See Also  Properties  Methods 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : HopAnalysisState Class

Glossary Item Box

The following tables list the members exposed by HopAnalysisState.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorHopAnalysisState ConstructorInitializes a new instance of the HopAnalysisState class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyFrequencyGets or sets the frequency (Hz) of this hopping analysis state.  —
Public PropertyToleranceGets or sets the tolerance (Hz) of this hopping analysis state.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodSerialize  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also