Keysight 89600 VSA .NET API
HopStateDetectionMode Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : HopStateDetectionMode Enumeration


Glossary Item Box

Determines how frequency hop state detection occurs in the measurement.

Syntax

Visual Basic (Declaration) 
Public Enum HopStateDetectionMode 
   Inherits System.Enum
C# 
public enum HopStateDetectionMode : System.Enum 
C++/CLI 
public enum class HopStateDetectionMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ManualHop state detection is turned on and hop states are entered manually.—
OffHop state detection is turned off.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also