| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property AcquisitionExtraSamples As Integer | |
| C# | |
|---|---|
public abstract int AcquisitionExtraSamples {get; set;} | |
Property Value
The default value is 100. The maximum isint.MaxValue, and the minimum is 0.If IsSelectedPulsesExtraDataIncluded is true, the analysis traces include extra data before and after the selected pulses. Normally the length of the extra data shown would be chosen so that the selected pulses are within the middle 80% of the trace. However, if the pulses are too near the beginning or end of the Acquisition Time trace, this may not be possible. To help provide the extra data samples in this case, extra samples equal to AcquisitionExtraSamples are acquired at the start and end of Acquisition Time.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00