Keysight 89600 VSA .NET API
AmplitudeDomain Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : AmplitudeDomain Property


Glossary Item Box

Gets or sets the amplitude domain used for determining rise/fall/pulse width thresholds (which are in units of percent).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AmplitudeDomain As AmplitudeDomain
C# 
public abstract AmplitudeDomain AmplitudeDomain {get; set;}
C++/CLI 
public:
abstract property AmplitudeDomain AmplitudeDomain {
   AmplitudeDomain get();
   void set (    AmplitudeDomain value);
}

Property Value

The default value is Voltage.

Remarks

This also affects the calculation of metrics, such as Ripple (%), Overshoot (%), or Droop (%).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also