Keysight 89600 VSA .NET API
CorrelationReferenceRegisterEndOffset Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : CorrelationReferenceRegisterEndOffset Property


Glossary Item Box

Gets or sets the end time offset used when getting the correlation reference from a data register.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CorrelationReferenceRegisterEndOffset As Double
C# 
public virtual double CorrelationReferenceRegisterEndOffset {get; set;}
C++/CLI 
public:
virtual property double CorrelationReferenceRegisterEndOffset {
   double get();
   void set (    double value);
}

Property Value

The units are seconds. The default value is 0.0.

Remarks

This specifies how far back from the end of the data register.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also