Gets or sets the start time offset used when getting the correlation reference from a data register.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property CorrelationReferenceRegisterStartOffset As Double |
| C# | |
|---|
public virtual double CorrelationReferenceRegisterStartOffset {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double CorrelationReferenceRegisterStartOffset {
double get();
void set ( double value);
} |
Property Value
The units are seconds. The default value is 0.0.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also