Gets or sets the phase shift angle for Custom BPSK.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property CustomBpskPhaseShift As Double |
| C# | |
|---|
public virtual double CustomBpskPhaseShift {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double CustomBpskPhaseShift {
double get();
void set ( double value);
} |
Property Value
The default value is 180 degree.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight PathWave 89600 VSA
Ver 25.00
See Also