Keysight 89600 VSA .NET API
FMFilterBandwidthFactor Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : FMFilterBandwidthFactor Property


Glossary Item Box

Gets or sets the FM filter bandwidth factor in percentage of measurement span.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FMFilterBandwidthFactor As Double
C# 
public abstract double FMFilterBandwidthFactor {get; set;}
C++/CLI 
public:
abstract property double FMFilterBandwidthFactor {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.05. The maximum is 0.5, and the minimum is 0.0008.

Remarks

This is the -3 dB bandwidth (where the filter response is 3.01 dB below an ideal straight-line differentiating filter).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also