Keysight 89600 VSA .NET API
GetDeinterleaveMaxFrequencies Method
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : GetDeinterleaveMaxFrequencies Method


Glossary Item Box

Gets the maximum frequency values for each emitter (Hz).

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetDeinterleaveMaxFrequencies() As Single()
C# 
public virtual float[] GetDeinterleaveMaxFrequencies()
C++/CLI 
public:
virtual array<float>^ GetDeinterleaveMaxFrequencies(); 

Return Value

An array of the maximum frequency values.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also