Keysight 89600 VSA .NET API
IsExtendedDemodBitsEnabled Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsExtendedDemodBitsEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the long modulated pulse automatically detect.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsExtendedDemodBitsEnabled As Boolean
C# 
public virtual bool IsExtendedDemodBitsEnabled {get; set;}
C++/CLI 
public:
virtual property bool IsExtendedDemodBitsEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

Long demodulation feature enable/disable properties. If value is true, Demodulation supports up to 1024 chips. Supported formats are BPSK and QPSK.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also