Keysight 89600 VSA .NET API
IsModulationTypeFrankCodeEnabled Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsModulationTypeFrankCodeEnabled Property


Glossary Item Box

Gets or sets a value indicating whether Frank Code modulation may be detected.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsModulationTypeFrankCodeEnabled As Boolean
C# 
public virtual bool IsModulationTypeFrankCodeEnabled {get; set;}
C++/CLI 
public:
virtual property bool IsModulationTypeFrankCodeEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also