Keysight 89600 VSA .NET API
IsPulseToPulseSameAsFrequencyPhaseAnalysisPart Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsPulseToPulseSameAsFrequencyPhaseAnalysisPart Property


Glossary Item Box

Gets or sets a value indicating whether pulse-to-pulse results are calculated on the same part of the pulse as frequency/phase results.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPulseToPulseSameAsFrequencyPhaseAnalysisPart As Boolean
C# 
public abstract bool IsPulseToPulseSameAsFrequencyPhaseAnalysisPart {get; set;}
C++/CLI 
public:
abstract property bool IsPulseToPulseSameAsFrequencyPhaseAnalysisPart {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also