Keysight 89600 VSA .NET API
IsSelectedPulsesUseAll Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : IsSelectedPulsesUseAll Property


Glossary Item Box

Gets or sets a value indicating whether all acquired pulses are selected.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsSelectedPulsesUseAll As Boolean
C# 
public abstract bool IsSelectedPulsesUseAll {get; set;}
C++/CLI 
public:
abstract property bool IsSelectedPulsesUseAll {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If false, then SelectedPulsesCount and SelectedPulsesStart determine which pulses are selected.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also