Gets or sets a value indicating whether to use the edges of the Top of the pulse in calculating the rise, fall, and pulse width thresholds.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property IsTopLevelCompensatedForDroop As Boolean |
| C# | |
|---|
public abstract bool IsTopLevelCompensatedForDroop {get; set;} |
| C++/CLI | |
|---|
public:
abstract property bool IsTopLevelCompensatedForDroop {
bool get();
void set ( bool value);
} |
Property Value
The default value is false.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also