Keysight 89600 VSA .NET API
ModulationFrequencyOffset Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : ModulationFrequencyOffset Property


Glossary Item Box

Gets or sets the manual modulation frequency offset for CW measurements

Syntax

Visual Basic (Declaration) 
Public Overridable Property ModulationFrequencyOffset As Double
C# 
public virtual double ModulationFrequencyOffset {get; set;}
C++/CLI 
public:
virtual property double ModulationFrequencyOffset {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.0.

Remarks

This is the modulation frequency offset used if IsModulationFrequencyOffsetAutomatic is false. It is determines the FM reference time trace value within the frequency/phase analysis region of every detected pulse.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00

See Also