Keysight 89600 VSA .NET API
PulseDroopMeasurementWidth Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : PulseDroopMeasurementWidth Property


Glossary Item Box

Gets or sets the portion of the pulse top used for calculation.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PulseDroopMeasurementWidth As Double
C# 
public virtual double PulseDroopMeasurementWidth {get; set;}
C++/CLI 
public:
virtual property double PulseDroopMeasurementWidth {
   double get();
   void set (    double value);
}

Property Value

The default values is 100%

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.00

See Also