Keysight 89600 VSA .NET API
PulseFrequencyPhaseChipMeasurementWidth Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : PulseFrequencyPhaseChipMeasurementWidth Property


Glossary Item Box

Gets or sets the portion of the middle of a chip used for frequency and phase calculations in Barker-modulated pulses.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PulseFrequencyPhaseChipMeasurementWidth As Double
C# 
public virtual double PulseFrequencyPhaseChipMeasurementWidth {get; set;}
C++/CLI 
public:
virtual property double PulseFrequencyPhaseChipMeasurementWidth {
   double get();
   void set (    double value);
}

Property Value

The default value is 75%.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00

See Also