Keysight 89600 VSA .NET API
PulseFrequencyPhaseMeasurementWidth Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : PulseFrequencyPhaseMeasurementWidth Property


Glossary Item Box

Gets or sets the portion of the middle of a pulse used for frequency and phase calculations in CW or linear FM pulses.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PulseFrequencyPhaseMeasurementWidth As Double
C# 
public abstract double PulseFrequencyPhaseMeasurementWidth {get; set;}
C++/CLI 
public:
abstract property double PulseFrequencyPhaseMeasurementWidth {
   double get();
   void set (    double value);
}

Property Value

The default value is 75%.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also